4. Software

The following sub-sections provide instructions for the installation of the Force Copilot software package. This allows you to get data from a force torque sensor.

4.1. Control with Universal Robots

Force Copilot contains many features to program and control the robot’s arm using a sensor’s force and torque readings. The package provides:

4.1.1. ActiveDrive Toolbar

The ActiveDrive Toolbar is automatically installed with the Force Copilot software Package. It enhances the guiding mode on Universal Robots by allowing the robot to be hand guided smoothly and easily towards a waypoint. The ActiveDrive feature is a great way to assist the Path recording described in the Path Recording section, by hand guiding the robot while recording a path.

Info

The Force Copilot software Package contains the ActiveDrive Toolbar. Therefore, the toolbar is automatically installed with the URCap Package.

Info

The ActiveDrive Toolbar can be installed and used without the URCap Package (refer to the UR Package without URCaps section for information on how to install the toolbar without the URCap).

Warning

Verify that the Force Torque Sensor is aligned with the robot arm using the dowel pin. This ensures that the Sensor’s axes are aligned with the robot and that the ActiveDrive feature will work correctly.

The robot speed set with the Speed slider will affect the speed at which the robot moves in the ActiveDrive mode. Verify and adjust the speed slider to the desired speed. It has to be greater than 50%.

4.1.1.1. Overview

Toolbar collapsed

Tap the ActiveDrive button to expand the toolbar.

Toolbar expanded

(Tap the mode selector to expand.)

ActiveDrive modes expanded

4.1.1.2. Features

Primary icon

Functionality name

Description

ActiveDrive

Tap to toggle between the expanded and collapsed ActiveDrive Toolbar. When grey, the functionality is not available. Tap the button to see why it is not available.

Start / Stop

Tap to start or stop ActiveDrive. ActiveDrive will automatically turn off after 30s of inactivity.

When started, ActiveDrive allows you to move the robot freely by applying forces on robot’s end-effector. This is different from the Free Drive feature on the robot, where you can move the robot arm.

Modes

Shows the current ActiveDrive mode. When tapping the icon, the available modes will appear and you can change to a different mode. ActiveDrive modes allow you to restrain the robot to specific movements.

Free

Free motion: all translations and rotations are allowed.

Scara

SCARA-style motion: all translations and horizontal rotation (twist) are allowed.

Translation

Translation motion: only translations are allowed. No rotation of the robot is possible in this mode.

Plane

Plane motion: horizontal translations and horizontal rotations (twist) are allowed (no vertical motions are allowed).

Drift Control

Tap this button to stop the robot from drifting (resets the sensor’s offset).

Speed

Motion speed control is toggled between fast and slow, allowing precise movement in slow motion.

The force torque sensor will switch to slow speed automatically whenever high forces are detected, for example, during an impact with an object.

Square robot

Aligns the tool center point (TCP) orientation with the robot base. Tap and hold this button to automatically move the end-effector to the closest orthogonal orientation of the base axis system (just try it, you will see!).

4.1.1.3. Error Messages Overview

The ActiveDrive Toolbar will be automatically collapsed and be grayed whenever one of the following situations occurs. In such cases, by tapping the ActiveDrive button, the following messages will appear:

4.1.2. Using the force and torque values

Force Torque Sensor functions are made available in the Universal Robots functions drop-down menu.

 

Fig. 4.1: Example of two reference frames for the express_force_in_frame(<T_from_to>,<wrench_from>) function

 

Info

Although displayed in real time in the Variables tab, the force and torque values can be seen in the Force Copilot Dashboard.

After the calibration has been completed, go to the FT 300 Dashboard to monitor the force and torque values in real time.

Prior to using the FT Sensor's data in the framework of a robot program, it is recommended to zero the sensor using the Zero sensor button.

 

Fig. 4.2: Force Copilot Dashboard with force and torque values displayed in real time.

4.1.3. Path Recording

The Force Copilot software package adds a Path feature in PolyScope which can be used to record paths directly by moving the robot. The ActiveDrive Toolbar is a great tool to use while recording a path, as it is an easy way to hand guide the robot’s end-effector. Path recording can be used for specific processes requiring complex paths (polishing, gluing, etc.) or more generally for any useful case that would require programming a high number of waypoints. The Path node offers options to modify the recorded path to change its speed and play the path backwards or relative to a variable start position.

How to add and record a path

  • On the PolyScope home page, tap Program Robot
  • Create an empty program or load an existing program

  • In the Program tab, select the Structure menu.
  • Select the URCaps submenu.
  • Tap the Path button

 

4.1.3.1. Overview

 

Path recording and visualization.

Path speed box.

Path options.

Warning section. Displayed whenever a setting results in a duration different than the original path duration.

When a Path node is empty (no path recorded), the only available button is the record button.

 

While recording a path, the only available button is the stop button.

When the speed of the original recording is modified using the speed slider, a warning message appears and the path time and speed information is updated.

4.1.3.2. Features*

Primary icon

Description

Starts and stops the path recording.

Press and hold in order to move the robot at the path’s start.

Press and hold in order to move the robot at the path’s end.

Press and hold in order to move the robot to the path’s start and play the path as it will be executed in the program.

If selected, the path is modified to play at a constant tool speed (linear speed at the tool center point). With this option, all pauses and hesitations (dead times) in the path will be removed.

If selected, the recorded path will be played backwards in the program. It can be useful if a path is copied and played backwards, resulting in a path played back and forth.

If selected, the path will be played relative to the current robot position when the program enters the path instruction.

This effectively offsets all the recorded path.

Displayed whenever a setting results in a duration different than the original path duration.

* When an icon is greyed, it means it is unavailable.

If you tap the record button when a path is already recorded in a node, a warning pop-up will ask if you want to overwrite the path (tap OK) or keep the previously recorded path (tap Cancel).

4.1.4. Insertion nodes

The Force Copilot software Package includes Insertion nodes, which can be used to perform spiral, rotational and linear movements to insert objects in holes or bores, or to make contact with a surface. It is an essential integration resource for streamlining robot programs in the framework of precise assembly applications.

When the task is performed by a human operator, the operator's fingers provide valuable feedback through the sense of touch, thus allowing the human to detect any resistance when trying to insert a pin in a hole, for instance. To a certain extent, Force Copilot gives that kind of sensitivity to the end effector.

 

How to add an Insertion node

 

Info

The parent Insertion node is automatically followed by a Zero Sensor child node.

4.1.4.1. Child nodes

 

 

  1. Spiral button to insert a Spiral child node
  2. Rotational button to insert a Rotational child node
  3. Linear button to insert a Linear child node

 

Spiral
Following a contact established between the object grasped by the end effector (or the end effector itself) and the corresponding mating part or surface, a spiral motion is engaged on a specific plane to find the path of least resistance according to the direction, speed, force, radius increment per turn and maximum radius parameters set by the user.

Rotational

Following a contact established between the object grasped by the end effector (or the effector itself) and the corresponding mating part or surface, a rotational motion is engaged on a specific plane to find the path of least resistance, according to the direction, speed, force, maximum torque and maximum rotation angle parameters set by the user.


Linear

Following the successful spiral, rotational or fortuitous location of a mating hole or bore, a linear motion is engaged at a certain speed until the force threshold or maximum travel distance is reached.

Features (Spiral)

The Spiral child node is packaged with an On error condition line to be populated with a program instruction when/if the error condition occurs. The potential sequence after the Spiral instruction is followed by a program halt, by default.

  1. Teach position button (Destination): Tapping this button saves the object's destination as a waypoint in the robot program
  2. Reference frame dropdown menu (Direction): Menu used to select the frame according to which the tool will move in space
  3. Axis dropdown menu (Direction): Menu used to select the direction in which the tool will go to reach the destination
  4. Advanced parameters box: Box that expands the advanced parameters menu when ticked
  5. Speed parameter: Textbox for the user to enter a speed value
  6. Force initiating spiral move parameter: Textbox for the user to enter a force threshold value that triggers the spiral move, after the part/tool has established contact with the mating part/surface
  7. Force initiating insertion parameter: Textbox for the user to enter a force drop value indicating that the part/tool has found the path of least resistance, prior to completing the insertion process
  8. Radius increment per turn parameter: Textbox for the user to enter the distance between each spiral turn on the spiral radius
  9. Enable peck mode box: Box that enables the retraction of the tool between points of contact
  10. Maximum radius (Error condition): Textbox for the user to enter the maximum radius of the spiral, considering that no path of least resistance has been found

 

Default values and units of measurement

Parameter

Unit of measurement

Default value

Reference frame (Direction)

N/A

Tool

Axis (Direction)

N/A

Z+

Speed

mm/s

5

Force initiating spiral move

N

10

Force initiating insertion

N

3

Radius increment per turn

mm

0.7

Maximum radius (Error condition)

mm

5

 

Features (Rotational)

 

  1. Teach position button (Destination): Tapping this button saves the object's destination as a waypoint in the robot program
  2. Reference frame dropdown menu (Direction): Menu used to select the frame according to which the tool will move in space
  3. Axis dropdown menu (Direction): Menu used to select the direction in which the tool will go to reach the destination
  4. Advanced parameters box: Box that expands the advanced parameters menu when ticked
  5. Linear speed parameter: Textbox for the user to enter a speed value for the approach motion towards the destination
  6. Force initiating rotation parameter: Textbox for the user to enter a force threshold value that triggers the rotation move, after the part/tool has established contact with the mating part/surface
  7. Rotation speed parameter: Textbox for the user to enter a speed value for the rotational (indexing) motion
  8. Maximum torque parameter: Textbox for the user to enter a torque threshold value used to prevent potential collision with objects during the rotational motion
  9. Enable peck mode box: Box that enables the retraction of the tool between points of contact
  10. Maximum rotation angle (Error condition): Textbox for the user to enter the maximum angle of the rotation motion, considering that no path of least resistance has been found

Default values and units of measurement

Parameter

Unit of measurement

Default value

Reference frame (Direction)

N/A

Tool

Axis (Direction)

N/A

Z+

Linear speed

mm/s

5

Force initiating rotation

N

10

Rotation speed

°/s

5

Maximum torque

Nm

1

Maximum rotation angle (Error condition)

°

45

 

Features (Linear)

  1. Reference frame dropdown menu (Direction): Menu used to select the frame according to which the tool will move in space
  2. Axis dropdown menu (Direction): Menu used to select the direction in which the tool will go to reach the destination
  3. Advanced parameters box: Box that expands the advanced parameters menu when ticked
  4. Speed parameter: Textbox for the user to enter a speed value for the approach motion towards the destination
  5. Force threshold parameter: Textbox for the user to enter a force threshold value that completes the linear motion
  6. Maximum travel distance (Error condition): Textbox for the user to enter the maximum distance value which, upon being reached, means the force threshold has never been reached in the linear motion

Parameter

Unit of measurement

Default value

Reference frame (Direction)

N/A

Tool

Axis (Direction)

N/A

Z+

Speed

mm/s

5

Force threshold

N

10

Maximum travel distance (Error condition)

mm

100

 

4.1.5. Find Surface node

The Force Copilot software package includes the Find Surface node, which is a great tool for machine tending and various other applications that require repeated accurate positioning of objects.

The default parameters of the function allow for a versatile demo or a quick test of the features while the advanced parameters make it a more customizable asset.

 

How to add a Find Surface node

  1. Direction relative to the tool dropdown menu: Menu used to select the direction of the linear motion, relative to the tool
  2. Zero Sensor Before Execution box: Box that inserts a Zero FT Sensor command right before the Find Surface instructions
  3. Advanced parameters box: Box that expands the advanced parameters menu when ticked
  4. Motion speed parameter: Textbox for the user to enter a speed value for the approach motion towards the destination
  5. Maximum distance traveled (Stop condition): Textbox for the user to enter the maximum distance value which, upon being reached, means the force threshold has never been reached in the linear motion
  6. Insert instruction textbox: Checkbox that inserts the corresponding stop condition in the robot program when ticked; its main function is to facilitate the programming and improve the user experience
  7. Force threshold (Stop condition): Textbox for the user to enter a force thershold value that completes the linear motion
  8. Insert instruction textbox: Checkbox that inserts the corresponding stop condition in the robot program when ticked; its main function is to facilitate the programming and improve the user experience

 

Parameter

Unit of measurement

Default value

Direction relative to the tool

N/A

Z+

Motion speed

mm/s

5

Maximum distance traveled (Stop condition)

mm

100

Force threshold (Stop condition)

N

10

 

Fig. 4.3: Find Surface node with stop condition(s)

4.1.6. Using the Force Torque Sensor's Data in Force Nodes

In order to use the FT Sensor's data in Force control mode for all Force nodes, go to the Configuration tab and check the corresponding box. This will feed the Sensor's force values to the UR Force mode as an alternative to UR's embedded force feedback.

4.1.7. Force Control Node

4.1.7.1. Overview

The Robotiq Force Control node is used to apply force and torque values along and around axes.

How to add a Force Control node

 

 

Warning

UR Move nodes (MoveL, MoveJ, MoveP) and Force nodes cannot be executed as child of the Robotiq Force Control node.

 

Tip

Where a UR Move node would normally be used, the user shall record a Robotiq Path emulating the desired Move.

In a situation where the user wants to make contact with a surface in accordance with the user-defined settings, a Wait instruction can be inserted as child of the Robotiq Force Control.

 

The Force Control node is primarily meant to be used with a Robotiq Path node.

With the various user-defined settings available, operators can use a force torque sensor to apply force/torque and thus follow irregular shapes and/or surfaces for applications such as polishing, deburring, finishing, dispensing, etc.

4.1.7.2. Features

Reference frame

The user can select a reference frame from a dropdown menu, as shown below.

The Tool reference frame uses the X, Y and Z axes of the end-effector to apply force and torque values in the appropriate direction.

On the other hand, the Base reference frame takes into consideration the X, Y and Z axes of the robot arm base.

Fig. 4.4: Force Control node with Reference Feature dropdown highlighted.

Parameters

  1. Enable control: each checkbox corresponds to the enablement of force feeding along an axis (upper three options) or torque feeding around an axis (lower three options)
  2. Force/Torque: depending on which options were checked at step 1, the corresponding textboxes here should be filled with the desired force/torque values
    1. Force values applied are in newtons (N) – the range allowed goes from -150 to +150 N
    2. Torque values applied are in newton-metre (Nm) – the range allowed goes from -50 to +50 N.

Info

Tapping the text boxes brings up a numpad used to enter the values.

  1. Stiffness: the stiffness settings act directly on the Sensor's directional compliance depending on the orientation of the end-effector and the axes selected at step 1.
    1. A stiffness value closer to 0% will provide greater compliance along/around the corresponding axis
    2. A stiffness value of 100% offers no compliance along/around the corresponding axis
  1. Deviation range: the deviation range limits the flexibility allowed along/around the corresponding axis.
    1. The deviation range along the X, Y and Z axes is measured in millimeters (mm) – the negative range allowed goes from -1000 mm to 0 mm while the positive range allowed goes from 0 mm to 1000 mm.
    2. The deviation range around the X, Y and Z axes is mesured in degrees (°) – the negative range allowed goes from
      -179° to 0° while the positive range allowed goes from 0° to 179°.

Example

In a situation where 10 N are applied exclusively along the Z-axis, with 20% stiffness along the X and Y axes, and a deviation range that goes from -50 mm to +50 mm along all axes...

 

Fig. 4.5: Deviation range - On the left, no deviation range has been entered. On the right, a deviation range of at least 15 degrees has been entered around the corresponding axis.

 

  1. Enable adaptive stiffness: this checkbox greys out the stiffness values in the boxes at step 3 since the Force Control calculates the rigidity of the surface/object with which the end-effector comes in contact. Thus, constant force/torque values are applied to surfaces with variable rigidity (e.g.: long, bent, bending or folded sheets or parts.

    When entering into contact with a surface for the first time, the end-effector will pull back for it has reached the force/torque value entered at steps 2a and/or 2b. It will then go back to the surface and apply the same force/torque values while pulling back less and less over time.

 

Fig. 4.6: End-effector experiencing adaptive stiffness upon repeated contact with a surface

 

Test

The Test button applies the user-defined settings of the Force Control node to the sensor, therefore moving along/around the corresponding axes, if the control had been enabled for the latter, regardless of other instructions entered before or after the Force Control node in the program tree.

 

4.1.8. Force Event

The Force Copilot software package includes Force Event, which can be used to perform a click detection or to wait for a specific force or torque.

 

How to add a Force Event function

 

 

  1. Wait for Force function
  2. Click detection function

Wait for Force

The Wait for force feature is used to detect a specific force or torque inside a Force Control node.

Click Detection

The Click Detection feature is used to detect a drop that is followed by a rise of a force or a torque.

4.1.8.1. Features (Click Detection)

The Click Detection feature monitors forces and torques throughout the nodes placed within it. This feature senses if a drop in the force or torque is then followed by a sudden rise, thus making a "click". If a click is detected within the Click detection node, the program then skips the remaining instruction lines that are included in the Click detection node. The program automatically goes to the following instruction.

Indeed, a program instruction can be added if no click is detected.

 

 

Tip

To perform a click button action, as shown by the animated gif, a Find Surface function has to be added up in the Click detection node.

 

4.1.8.2. Features (Wait for Force)

The Wait for Force feature is used to detect a specific force or torque inside a Force Control node. The program waits until the force or torque is reached prior to the program continuation. The values are defined by the Force Control's force and torque parameters. To be sure the program is not incessantly running, a Timeout option is available.

 

4.1.9. Collision Detection

The Collision Detection feature is used to stop a program when the forces and the torques, monitored by the FT Sensor , exceed the defined limits. By default, the program does not monitor forces and torques.

How to add a Collision Detection

.

The Collision Detection feature in the installation tab can be configured to start the monitoring upon every robot program start. On the other hand, the Collision Detection node in the Program tab starts a thread that runs in parallel with the rest of the robot program. If the Stop monitoring option is selected in the Collision Detection node, the thread stops and the program continues without monitoring the force or the torque.

 

 

4.1.10. Multipoint Path Node

The Multipoint Path node is an advanced version of the Path node, combining complex trajectory recording and point-to-point teaching, with the option to define each segment as a straight line or as a curve.

Tip

Try inserting a Multipoint Path node in a Robotiq Force Control node. The former will perform the movements that were taught while taking into consideration the parameters set in the latter.

How to add a Multipoint Path node

 

Fig. 4.7: Multipoint Path node (empty)

 

Info

Please note that a Multipoint Path parent node is always followed by a MoveJ command leading to the starting waypoint of the path sequence.

 

4.1.10.1. How to set up a Multipoint Path

Step 1

 

At this point, the interface will look like this:

  1. Tap the Edit button to open the UR waypoint interface and adjust the position of the robot arm (this works for every waypoint of the Multipoint Path)
  2. Tap the Delete button to cancel the waypoint (deleting the starting waypoint will turn it to unsassigned)
  3. Tap and hold the Move here button to make the robot arm travel to the corresponding waypoint
  4. Tap the Add line button to let the system know that a straight line will be linking the current waypoint and the next waypoint
  5. Tap the Add curve button to let the system know that a curve will be linking the current waypoint and the next waypoint

Important

Whether the path is made of straight lines, curves or a mix of both, it inevitably passes through each waypoint set by the user.

Important

The curve segments are not generated and/or represented according to a spline model; they are rather based on Bézier curves.

Info

For describing the continuity of the curves used in the Multipoint Path node, control points are generated on the bisector of each waypoint junction (angle). Curves are therefore tangent to those bisectors.

Step 2

 

Fig. 4.8: Multipoint Path interface with Line/Curve options.

Caution

Adding several waypoints (lines or curves) without moving the robot in between them will result in the generation of identical waypoints.

In order to remedy this situation, the user can edit each waypoint created and adjust its position.

Tip

You can toggle at any time between the Line to waypoint and Curve to waypoint options.

Select the waypoint in the program tree and tap the appropriate radio button in the Command tab.

Repeat step 2 until you complete your Multipoint Path.

Fig. 4.9: Representation of a six-waypoint Multipoint Path with both curves and straight lines.

4.2. Development Package

The Robotiq Force Torque Sensor development package can be downloaded at support.robotiq.com.

 

4.2.1. Distribution License

The development package is distributed under the New BSD license, which is a permissive free software license. In short, the provided code can be used in any project without any restriction regarding its use (commercial or not). If it is included in a software, this software does not need to be open-source. However, the code is provided "as is" without any liability from Robotiq and some restrictions apply regarding the distribution of the code and the use of the Robotiq name.

The terms of the license (included in each source file) are described here:

Software License Agreement (BSD License)
Copyright (c) 2014, Robotiq, Inc. All rights reserved.
Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions are met:
- Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.
- Redistributions in binary form must reproduce the above
copyright notice, this list of conditions and the following
disclaimer in the documentation and/or other materials provided
with the distribution.
- Neither the name of Robotiq, Inc. nor the names of its
contributors may be used to endorse or promote products derived
from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
"AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN
ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
POSSIBILITY OF SUCH DAMAGE.

4.2.2. Linux

4.2.2.1. Package Files – Description

The development package is structured with the following files and directories architecture (non-Linux files and directories are ignored in this section):

Caution

When started, the provided software will scan all ports in the system (ttySx and ttyUSBx) to find a compatible Robotiq device. It uses the Linux utility "fuser" to determine if the port is already opened. This section of code can be modified by the user if necessary to avoid the scanning of ports (for example, if another device would become confused when receiving a message that it cannot understand).

4.2.2.2. Procedure to Compile and Test the Provided Source Code

This procedure explains how to compile the source code and verify that the sensor data is properly read.

  1. Unzip the package in the home folder, for example in the folder ~/driver/
  2. Open a terminal and enter the package directory using the following command:

    rd@debian:~/$ cd driver
  3. Use Make to compile the application:

    rd@debian:~/$ make linux
  4. In order to have access to the virtual serial COM port, add the used username to the group dialout:

    rd@debian:~/$ sudo usermod -a -G dialout username
  5. It is required to log out (or reboot) the session in order for the group change to become effective.
  6. Make sure that the sensor is properly powered and that the data signals are connected to the development PC using the provided RS485 to USB converter. A new device named ttyUSBx should be present in /dev, which can be verified with the following command:

    rd@debian:~/$ ls -l /dev | grep ttyUSB
  7. In a terminal, go to the ~/driver/Linux/bin folder and execute the demo application using the following command:

    rd@debian:~/driver/Linux/bin/$ ./driverSensor
  8. After 1-2 seconds, the sensor data should start showing up in the terminal as a vector of 6 floats with data in the (Fx, Fy, Fz, Mx, My, Mz) format.

 

Fig. 4.10: Sensor Data Acquisition.

 

4.2.2.3. Adapt to a User Application

In practice, the provided source code will be adapted to either: be incorporated with a custom application or to communicate with one. At this point, the main.c file should be adapted according to the guideline comments inserted in the code.

Caution

Please note that Robotiq can only support our customers in making sure they can compile and test the provided code as is.

No support can be provided for the integration of the provided source code into a custom application.

4.2.3. Windows

4.2.3.1. Package Files – Description

The development package is structured with the following files and directories architecture (non-Windows files and directories are ignored in this section):

4.2.3.2. Procedure to Compile and Test the Provided Source Code

This procedure explains how to install MinGW, compile the provided source code and verify that the sensor data is properly read.

  1. Unzip the package in the desired directory.
  2. If it is not already installed, download MinGW at http://www.mingw.org/. Download the installer "mingw-get-setup.exe".
  3. Install MinGW by running "mingw-get-setup.exe" and save the default installation path.
  4. Open "MinGW installation manager".
  5. Select "mingw-developer-toolkit" in the "Basic setup" tab and click "Mark for Installation".
  6. Select "mingw32-binutils" in the "All packages" tab and click "Mark for Installation".
  7. In the menu "Installation", click "Apply changes". This will install the required packages to compose the software using Make.
  8. In the Windows directory, run the compiler.bat file. This will build your application.
  9. Run the application "driverSensor" located in the "Windows/bin/" folder.
  10. After 1-2 seconds, the sensor data should start showing up in the command window as a vector of 6 floats with data in the (Fx, Fy, Fz, Mx, My, Mz) format.

Fig. 4.11: Sensor Data Acquisition Under Windows.

4.2.3.3. Adapt to a User Application

In practice, the provided source code will be adapted to either: be incorporated with a custom application or to communicate with one. At this point, the main.c file should be adapted according to the suggested comments inserted in the code.

Caution

Please note that Robotiq can only support our customers in making sure they can compile and test the provided code as is.

No support can be provided for the integration of the provided source code into a custom application.

4.3. Visual Demo Software

The Visual Demo Software is used to demonstrate the ability of the FT Sensor to read force and moment. It is not intended to be used for programming or to save or use data. It can also be used to calibrate the Sensor. Please refer to the Calibration Procedure for the Visual Demo Software (PC) section for the calibration procedure.

4.3.1. Software Package Installation

  1. Make sure that you have the latest version of the Visual Demo Software, which can be found at support.robotiq.com.

  2. Copy all the files of this folder onto a PC.
  3. Connect the USB connector to the converter attached to the PC. Important : The Sensor must NOT be powered at this time.
  4. Wait while the driver(s) install. After all the drivers have been installed.
  5. Plug the Sensor cable into the Sensor.
  6. Connect the Sensor cable to the power supply.
  7. Launch the demo application.

  8. You should see a COM port in green with a serial number, showing the Sensor connected to the PC. Click on it.

By going into the Sensor Data tab, you can now see in real time the force and moment applied on the FT Sensor.

4.4. Serial Communication

The FT Sensor uses two communication modes, Modbus RTU and data stream. The Modbus RTU communication mode is used to obtain information on the Sensor, like its firmware version. The data stream mode is used to obtain data from the Sensor.

Info

It is recommended to use the FT Sensor data stream to obtain faster data acquisition.

 

Caution

Modbus RTU can be used to obtain data, but will result in a slower data acquisition frequency.

 

Info

In both modes, force and torque data from the Sensor will be in 16-bits signed integer format.

 

4.4.1. Modbus RTU

The FT Sensor can be controlled over USB using an ACC-ADT-USB-RS485 signal converter. This section is intended to provide guidelines for setting up a Modbus scanner that will adequately communicate with the Sensor.

For a general introduction to Modbus RTU and for details regarding the CRC algorithm, the reader is invited to read the Modbus over serial line specification and implementation guide available at: : http://www.modbus.org/docs/Modbus_over_serial_line_V1_02.pdf.

For debugging purposes, the reader is also invited to download one of many free Modbus scanners such as the CAS Modbus Scanner from Chipkin Automation Systems available at: http://www.store.chipkin.com/products/tools/cas-modbus-scanner.

Info

Modbus RTU is a communication protocol based on Big Endian byte order. Therefore, the 16-bit register addresses are transmitted with the most significant byte first. However, the data port is, in the case of Robotiq products, based on the Little Endian byte order. As such, the data parts of Modbus RTU messages are sent with the less significant byte first.

Tip

Modbus RTU specification and details can be found at www.modbus.org

4.4.1.1. Connection Setup

The following table describes the connection requirements for controlling the Sensor using the Modbus RTU protocol:

Propriety

Value

Baudrate (bps)

19,200

Data bits

8

Stop bit

1

Parity

None

Supported Functions

Read Holding Register (FC03)

Preset Multiple Register (FC16)

Slave ID

0x0009 (9)

 

In Modbus RTU you can obtain the following information:

Information

Register

Production year-

514

Serial number

510 to 513

Force X (N) = value / 100

180

Force Y (N) = value / 100

181

Force Z (N) = value / 100

182

Moment X (Nm) = value / 1000

183

Moment Y(Nm) = value / 1000

184

Moment Z (Nm) = value / 1000

185

Acceleration X (g) = value / 1000

190

Acceleration Y (g) = value / 1000

191

Acceleration Z (g) = value / 1000

192

4.4.1.2. Read Holding Register (FC03)

Function code 03 (FC03) is used to read the status of the Sensor (robot input). Examples of such data is the display of the current force and torque values.

Example of FC03 Read Function:

To get Fx, you need to read (03) the register 180 (00B4) in device ID 9 (09).

Request is: 09 03 00 B4 00 01 C5 64

Hex format: 0x09 0x03 0x00 0xB4 0x00 0x01 0xC5 0x64

Bits

Description

09

SlaveID

03

Function Code 03 (Read Holding Register)

00B4

Address of the first requested register

0001

Number of registers requested (1)

C564

Cycle Redundancy Check (CRC)

 

To get all 6 force/torque values at once, you need to read (03) six registers (0006), starting with register 180 (00B4) in device ID 9 (09).

Request is: 09 03 00 B4 00 06 04 A6

Hex format: 0x09 0x03 0x00 0xB4 0x00 0x06 0x84 0xA6

Bits

Description

09

SlaveID

03

Function Code 03 (Read Holding Register)

00B4

Address of the first requested register

0006

Number of registers requested (6)

04A6

Cycle Redundancy Check (CRC)

 

4.4.2. Data Stream

Data stream mode is the recommended method of obtaining data from the Sensor. Once initiated, the Sensor will stream force and moment data continuously until communication is interrupted by the user.

Tip

To start the data stream, write 0x0200 in register 410.

For a setup over Universal Robots, Data stream will be accessible on TCP port 63351 of your machine.

Tip

With a Universal Robot, you can access the data stream using the documentation available at UR : Remote Control Via TCP/IP - 16496

To stop the data stream, communication must be interrupted by sending a series of 0xff characters to the Sensor. Sending for about 0.5s (50 times) will ensure that the Sensor stops the stream.

When the stream is started, 16 bytes messages are sent by the sensor at 100Hz using this format:

<0x20><0x4e><LSB_data1><MSB_data1> ... <LSB_data6><MSB_data6><LSB_crc><MSB_crc>

With dataX being a 16-bits signed integer defined as:

Data

Value meaning

data1

Fx * 100 (N)

data2

Fy * 100 (N)

data3

Fz * 100 (N)

data4

Mx * 1000 (Nm)

data5

My * 1000 (Nm)

data6

Mz * 1000 (Nm)

The CRC is computed using a standard 16-bits modbus CRC (see http://www.ccontrolsys.com/w/How_to_Compute_the_Modbus_RTU_Message_CRC).

 

4.4.2.1. Preset Multiple Registers (FC16)

Function code 16 (FC16) is used to activate functionalities of the Gripper (robot output). A common example is the initialization of data streaming.

Example of setting multiple registers (FC16):

To initialize the data stream, 0x0200 must be written with the function 16 (0x10) in register 410 (019A).

Request is: 09 10 01 9A 00 01 02 02 00 CD CA

Hex format: 0x09 0x10 0x01 0x9A 0x00 0x01 0x02 0x02 0x00 0xCD 0xCA

Bits

Description

09

SlaveID

10

Function Code 16 (Preset Multiple Registers)

019A

Address of the first register

0001

Number of registers requested (1)

02

Number of data bytes to follow (1 registers x 2 bytes/register = 2 bytes)

0200

Value written to register 0x019A

CDCA

Cycle Redundancy Check (CRC)