7. Specifications

Caution

The following manual uses the metric system, unless specified, all dimensions are in millimeters.

The following sub-sections provide data on the various specifications for the Robotiq 2-Finger 85 and 140 Adaptive Grippers.

7.1. Mechanical Specifications of Wrist Camera

Fig. 7-1: Wrist Camera's dimensions.

 

Specification

Value

Maximum load

10 kg

40 Nm

Weight (without tool plate)

160 g

Weight (with tool plate)

230 g

Added height (without tool plate, for use with 2-Finger Gripper)

13.5 mm

Global thickness (without tool plate)

22.4 mm

Added height (with tool plate)

23.5 mm

Global thickness (with tool plate)

29.5 mm

Wrist Camera's mechanical specifications.

 

Photographic sensor

Respecting Universal Robots's axes system, the photographic sensor's is located at [0mm; 35.7mm; -0.1mm] of the tool flange on which the camera is mounted. The line of sight passes through this point and is at 30° from the Z-axis.

7.1.1. Center of Mass and Moment of Inertia

The coordinate system used to calculate the moment of inertia and center of mass of the Wrist Camera is the base of the Camera which correspond to the UR tool flange reference [0,0,0].

Here is the approximate position for the center of mass. It has been calculated for the camera itself and for combinations with other Robotiq products. The camera's tool plate is included when the gripper is not mounted on the Wrist Camera.

 

Combination

x (mm)

y (mm)

z (mm)

Mass (grams)

-

0

5

9

230

FT 300

0 2

30

530

2-Finger 85

0 1

58

975

2-Finger 140

0

1

66

1040

FT 300 and 2-Finger 85

0

1

77

1275

FT 300 and 2-Finger 140

0

1

85

1340

Here is the approximate moment of inertia matrix for the Wrist Camera:

Inertia Matrix

Metric value
(kg * mm2)

Imperial value
(lb * in2)

lxx

lxy

lxz

111

0

0

0.38

0

0

lyx

lyy

lyz

0

70

3

0

0.24

0.01

lzx

lzy

lzz

0

3

165

0

0.01

0.56

 

Fig. 7-2: Center of Mass with and without the toolplate.

7.2. Electrical rating & performance of Wrist Camera

Robotiq recommends you supply the Wrist Camera from the Universal Robots controller power supply as shown in the Electrical Setup section; if for any reasons you cannot do so, here are the electrical specifications of the Camera:

 

Specification

Value

Operating supply voltage

24 V DC ±20%

Quiescent power (minimum power consumption)

1 W

Maximum power

22 W

Communication interface

USB 2.0

Here are the Wrist Camera's specifications:

 

Specification

Value

Maximum resolution

5 Mpx at 2 fps (2560 X 1920)

Maximum frame rate

30 fps at 0.3 Mpx (640 X 480)

Active array size

2592 X 1944

Focus range

70 mm to infinity

Integrated lighting

6 LED diffuse white light

Autofocus technology

Liquid lense

7.3. Vision System Specifications

Accuracy

The accuracy of the vision system is as described in the table below and depends on the robot model used. It is valid for the area where the calibration board was located during the calibration process.

 

Robot Model

Accuracy

UR3 +/- 2mm
UR5 +/- 3mm
UR10 +/- 3mm

Fig. 7-3: Accuracy of the vision system.

 

Calibration board position

Fig. 7-4: Calibration board position.

Specification

Value

UR3

UR5

UR10

Minimum board distance (cm) 26 34 42
Maximum board distance (cm) 42 70 98

Tips

Snapshot Position will determine the field of view, notice that the calibration step position does not have to be the same as Snapshot position. Thus, you can have a small field of view, then move back for calibration step.

Field of view

 

Specification

Value

UR3

UR5

UR10

Maximum board distance (cm) 36 x 27 64 x 48 100 x 75
Minimum board distance (cm) 10 x 7.5 10 x 7.5 10 x 7.5

Info

Field of view is (FoV) determined by Snapshot position. To get the minimum FoV, the camera must be placed at 7 cm above the work plane.

Part dimensions

The maximum part size that can be detected by the Wrist Camera is 60% field of view's dimension. The minimum is 10%, no matter the robot or the field of view size.

Fig. 7-5: Maximum and minimum part size.

The part must not be higher than its smallest dimension (width or length) : maximum of 1:1 ratio.

Fig. 7-6: Maximum part height.

 

Info

Part height ratio is taken between the maximum part height at any point and the minimum dimension present on part contour, width or length.

Background contrast

To ensure a good model and part detection from the Vision system, you should use a background that has a high color contrast with the part to be detected. You must choose colors that are apart horizontally on the HSV cone shown below. Therefore, a change in value (intensity) only does not represent a good contrast. There has to be a great difference in hue and saturation to obtain a good object model from the object teaching wizard. You can use either the yellow or pink side of the colored background provided with the camera kit. If required, use a different colored background to teach your part.

 

Fig. 7-7: HSV color cone.